A COMPLETE HILTI TOOLKIT FOR PUNCHING SHEAR STRENGTHENING OF EXISTING CONCRETE STRUCTURES

Rohan Sar
Reading time: < 10 minutes
Article

Searching for effective methods to strengthen concrete deficient in punching shear? Hilti has you covered.

Software & Services
Structural Connections
Structural Strengthening

A Background to Strengthening

Over the last two decades, the construction industry has come under increasing pressure to reduce its environmental footprint and reuse existing building stock to meet growing socio-economic demands, particularly in urban environments where a sizeable proportion of reinforced concrete buildings and bridges are at the end of their service life and need either refurbishment or demolition. Besides end of service life, a few causes of strengthening existing structures may include:

  • A change in use or occupancy,

  • An expansion of the building’s footprint,

  • Additional floors in dense urban environments that makes expanding horizontally is not viable,

  • The introduction of new building codes,

  • The presence of errors or other deficiencies in the original construction, and

  • The need to address other durability issues caused by known hazards such as fire and earthquake.

The choice to strengthen the existing structure or demolish and rebuild is not always easy and depends on the current condition of the structure, the client’s brief, and the structure’s cultural, historical, and societal importance. If the structural engineer determines that strengthening the entire structure is possible, evidence suggests a 15-70% faster turnaround time (defined as the time between stopping activity in the building or on the bridge and returning it to service) as compared to demolishing and building afresh. Besides saving time, strengthening the structure may achieve a 10-75% reduction in the resource burden through savings in labor and material, directly impacting the structure’s environmental and carbon footprint [1]. A faster return and a lower initial investment are also vital considerations for clients.

Solutions for Strengthening and the Selection Process

However, these potential savings are strongly predicated upon the structural engineer’s ability to select and the construction industry’s ability to provide and install appropriate strengthening solutions that address identified local and / or global deficiencies. While most strengthening projects will usually incorporate multiple solutions, some are ruled out due to architectural, operational, or geometrical limitations, a lack of knowledge in design and / or execution, unavailability of appropriate equipment, which narrows the list of potential solutions. This selection is further influenced by the advantages and disadvantages accompanying these solutions and are not “silver bullets” miraculously resolving structural deficiencies. Adding another layer of complexity is the potential for flawed implementation of these solutions that may lead to strengthening a particular part of the structure but weakening another, illustrated by the following two examples, one at a local and the other at the global level:

  • Local: thickening the slab with a concrete overlay but ignoring the additional loads on the supporting beams.

  • Global: a high concentration of shear infill walls on one side of the structure increasing the load demand on the other side, achieving the opposite effect.

At a “local” level, deficiencies may include the individual concrete members such as beams, columns, slabs, walls, and foundations lacking sufficient resistance to preclude failure in tension, compression, bending, shear, punching shear, torsion, and other effects caused by new loading demands. Solutions for individual members include, among others:

  • Concrete overlays or jackets as seen in Figure 1,

  • Post-installed reinforcement,

  • Steel jackets,

  • Near surface mounted (NSM) or bonded plates,

  • Fibre-reinforced polymer (FRP) wraps and strips,

  • External post-tensioning.

Reinforced concrete columns in a parking structure are wrapped with steel rebar cages during construction.

Figure 1: An example of concrete overlay / jacketing in columns

Strengthening on a “global” level typically includes addressing issues related to the whole structure, such as seismic, fire, fatigue, and wind by introducing solutions such as:

  • Shear infill walls as shown in Figure 2,

  • Steel braces,

  • Micro-piles,

  • Base-isolation,

  • Energy dissipation / damping devices.

Concrete shear wall under construction inside a building, with vertical rebar protruding at the top, temporary wooden formwork, and diagonal braces supporting the structure.

Figure 2: Example of a shear-infill wall between columns

Strengthening Concrete Slab and Foundations Deficient in Punching Shear

Assuming a building previously housing offices now changed to commercial use from a change in ownership, higher footfall will increase load on, say, the floor that must be resisted by all structural components – slabs, columns, and the foundations. Typically, after verification, an engineer may find that a flat slab may lack sufficient resistance in both bending and punching shear or, in some cases, only punching shear. Recall that in most design standards, such as Section 6.4 of EN 1992-1-1:2004 [2], the resistance of a concrete member in punching shear depends on the following five parameters:

  • Concrete strength,

  • Effective depth to the flexural reinforcement from the top of the compression fiber,

  • Size of the support and the control perimeter

  • The amount of longitudinal reinforcement

  • The amount of punching shear reinforcement

Employing a range of potentially available “local”-level solutions to improve one or several of these parameters enhances punching shear resistance by varying amounts, yet this incurs a trade-off in terms of invasiveness, cost, availability, and other parameters. Some modifications may not be even feasible, such as increasing the concrete strength of an existing beam. Others, such as adding more supports through additional columns to reduce punching shear demands will require load transfer to the foundations. Therefore, the Hilti range of solutions to enhance parameters (1) to (5) is summarized in Table 1:

Parameter

Strengthening Solution

How does Hilti assist?

Increasing the slab thickness & effective depth

Concrete Overlay

Hilti HCC-series: HCC-HUS4, HCC-U, HCC-K, and HCC-B

Increase the effective depth to flexural reinforcement

Steel plates

Concrete Overlay with Post-installed rebar

Hilti post-installed anchors for steel plates

Hilti HCC-series and post-installed rebar

Increasing the size of the support

Post-installed steel capital or struts

Post-installed column heads (drop panels)

Hilti post-installed anchors

Hilti post-installed rebar

Increase longitudinal reinforcement

Concrete Overlay

Hilti HCC-series: HCC-HUS4, HCC-U, HCC-K, and HCC-B and post-installed rebar

Increase punching shear reinforcement

Post-installed punching shear reinforcement

Hilti HZA-P

HIT-Punching Shear with HAS(-U) rods

Table 1: Potential solutions to strengthen concrete deficient in punching shear

Directly increasing the amount of punching reinforcement results in a proportional increase of the punching resistance, and the solutions available presently in the industry are typically minimally invasive and will reduce disruption to other members. The use of all other solutions typically results in an under-proportional increase to the punching resistance, apart from concrete overlay, which is accompanied by its own trade-offs.

Post-Installed Punching Shear Reinforcement to Increase Resistance

In recent years, the development and sufficient maturity of post-installed anchoring technology have led its use in applications beyond steel-to-concrete fastenings and concrete-to-concrete connections. One use in strengthening is in concrete overlay where both bonded and mechanical fasteners function to reinforce the interface between the existing and new concrete.

Another use of the bonded anchor system in strengthening is in a recently developed Hilti strengthening solution “HIT-Punching Shear” which directly increases the resistance to punching shear loading of reinforcement concrete members, as illustrated in Figure 3, akin to cast-in stirrups.

3D diagram of a concrete slab-to-wall connection showing multiple installed anchors arranged across the slab, with embedded reinforcing bars and drilled anchor holes highlighted.

Figure 3: Hilti HIT-RE 500 V4, HAS(-U) rods, and filling set used as post-installed punching shear reinforcement

This solution is installed in a similar way to a bonded anchor: i.e., drilling to a fixed embedment depth perpendicular to the concrete surface, thoroughly cleaning the debris from the boreholes, and injecting the mortar and then inserting the rods. Once the mortar cures, the nuts can be torqued up to a maximum specified value.

Note: Unless explicitly considered in design, drilling and cutting through the flexural reinforcement should be avoided wherever possible to prevent further weakening of the structure. If this cannot be avoided, for instance to facilitate drilling in densely reinforced areas, additional measures with the explicit agreement of the Engineer-in-Charge of design are required to compensate for a loss of flexural reinforcement.

New Hilti "HIT-Punching Shear" Strengthening Solution

The new Hilti HIT-Punching Shear strengthening solution consists of the following components:

Infographic of a concrete anchoring system showing anchor layouts, rebar integration, installation steps, tools, and materials including injectable mortar and threaded steel rods.

The solution pairs the HIT-RE 500 V4 injection mortar with Hilti HAS series of threaded rods in sizes M12, M16, M20, and M24, each available in carbon- and stainless-steel for indoor or outdoor use. The steel elements are completed by the Hilti Filling Set that consists of a sealing and spherical washer, a nut, and an optional locknut, also available in both carbon- and stainless-steel for each rod diameter.

The versatility of this system covers the following parameters:

  • Slab thickness between 200-1100 mm, with a minimum effective depth of 160 mm.

  • Installation from top or bottom side of the slab with defined rod length ranges as function of the slab thickness and rod diameter.

  • Concrete strength between C20/25 & C50/60.

  • Dry or water-saturated concrete, and in waterfilled holes.

  • Maximum short- and long-term temperatures of +40°C and +24°C, respectively.

  • Members subjected to static and quasi-static loading.

Flexibility in Your Hands - Leverage the Power of PROFIS Engineering

Hilti’s cloud-based design software PROFIS Engineering includes a new dedicated module for assessing and strengthening concrete members deficient in punching shear that assists structural engineers when evaluating the resistance of existing members and strengthening them, thereby ensuring a safer and more efficient workflow. The new PROFIS Engineering Punching Shear Strengthening module enables:

  • Selection between rectangular and circular column, wall ends, and wall corners on slabs and definition of its material properties & geometry.

  • Verification of the existing concrete’s resistance to EN 1992-1-1:2004.

  • Strengthening according to aBG Z.15-5.387 [5] in conjunction with DIN EN 1992-1-1/NA:2013, with a choice of four reinforcing diameters in carbon- or stainless-steel and a free input of the spacing and edge distances.

  • Free manual input of the radial spacings and the number of strengthening elements in each perimeter.

  • Generation of a comprehensive design report with all verifications, reinforcement detailing, and installation instructions.

Screenshot of engineering design software showing slab strengthening layout with post-installed anchors arranged in perimeters, along with input settings and verification results.

Summary

Transforming and reusing older structures can offer many advantages over new build ones, with each structure requiring fulfilment of specific objectives when strengthened. Based on the chosen design philosophy, the structural engineer can address punching shear deficiencies in slabs and foundations through various methods, some less invasive than others. The use of post-installed punching shear reinforcement, such as Hilti’s solution of HAS(-U) threaded rods with the HIT-RE 500 V4 mortar, is a novel example of a minimally invasive method that can significantly enhance the punching shear resistance of a structural member.

Suitably assessed and granted a general construction technique permit (aBG) as a system by DIBt, engineers can use a familiar Eurocode 2-based design approach integrated into Hilti’s PROFIS Engineering Suite to arrive at a feasible solution by selecting between the key design parameters such as diameter and spacing. With an intuitive interface, the new Punching Shear Strengthening module assists engineers by saving time during the design phase, bringing value to their clients while also contributing to a safer and more resilient built environment.

To know more, refer to our Whitepaper [4] that expands on this article.

For a walkthrough of the PROFIS Engineering module watch this video now

To start designing, visit https://profisengineering.hilti.com/

PROFIS Engineering Suite is a user-friendly, cloud-based software that makes designing structural connections faster and easier. Check out the full offering below.

PROFIS Engineering Software Suite

References

  1. N. Addy, “Making sustainable refurbishment of existing buildings financially viable”, in Sustainable Retrofitting of Commercial Buildings - Cool Climates, S. Burton, Ed., Abingdon, Routledge, 2015, pp. 57-73.

  2. EN 1992-1-1:2004: “Eurocode 2 - Design of concrete structures - Part 1-1: General rules and rules for buildings”, Brussels: CEN, 2004.

  3. “Concrete-to-Concrete Connections Handbook”, Hilti AG, Liechtenstein, May 2024.

  4. “Whitepaper on Shear-friction Applications and Concrete Overlays”, Hilti AG, Liechtenstein, Dec. 2023.

  5. Deutsches Institut für Bautechnik, “Z-15.5-387 - Hilti Durchstanzverstärkungssystem mit Hilti HIT-RE 500 V4”, DIBt, Berlin, 2025.