To use your consumable credit voucher
- Place a new order for consumable products directly via our website using your Hilti Account. The new order for consumable products has to be in an amount that is the same or greater than the credit voucher amount. Voucher may not be used on the same qualifying purchase that earned you the voucher or any prior purchases or outstanding balances.
- Click here to open the voucher redemption link or refer to the link on the voucher confirmation email to open the voucher redemption page
- Enter your Company Name that registered in our system
- Enter your Consumable Order Number. You can find this number on your confirmation email of the consumable products order you just placed
- Enter your Voucher Number stated in your Voucher confirmation email and your email address
- You will receive an invoice for the full amount of the consumable order. You will receive a credit memo for the voucher amount once you place your new consumable qualifying order. You will receive your credit memo within five business days.
- Consumable Credit Vouchers must be used within 90 days of date of issue.
Terms of Use
This Consumable Credit Voucher is only valid for Hilti customers with a credit-approved account that is in good standing. It is non-transferable and has no cash value and is valid only for a qualified consumable purchase within 90 days of issue. This offer may not be combined with any other offer. The consumable voucher can only be redeemed in a single transaction. Tools and accessories are not considered consumable items. Consumables are products that are used up during an application. This includes power tool accessories such as drill bits, abrasive blades, saw blades and impact wrench sockets. Consumables also include products installed during an application: fasteners, firestop, filler foam, strut, threaded rod This is not your credit memo. A credit memo will be issued after you place a valid consumable products purchase referencing the above voucher number.