BARRY DRIVE BRIDGE UPGRADE, ACT
Environmental challenges solved with Hilti SAFEset dustless drilling solution.

SAFEset Technology
SafeSet Technology is a major advancement for the construction industry, having increased drilling productivity while also improving reliability in setting chemical anchors. The new hollow drill bit means that borehole drilling can occur 10 to 20 per cent faster than with a traditional helix drill bit. This accounts for an estimated time saving of up to 90 seconds per hole. The cleaning process of repeatedly blowing and brushing out the holes is not only labour intensive but can also compromise the anchor capacity if not done correctly.
Jared Hawkins, Project Manager for Hawkins Civil said that, "the system worked beyond our expectations. It impressed our client, as well as the Local Environmental Protection Agency. Hawkins Civil has relied on Hilti products for years and this system did not disappoint. The productivity gains were as good as promised, and the service was exceptional."
An All-round success for the environment

The project included the installation of approximately 2,000 anchors, along with carbon fibre reinforcements to increase the strength of the bridge deck. All drilling was done with a Hilti-designed system that utilised an overhead drill press designed and manufactured locally by Baxter Engineering. The ACT Environmental Protection Agency inspected the site numerous times and commented on the efficiency of the system and quality of the environmental controls. Furthermore, the system as a whole, including the drills, bits, vacuums, glues and incidentals, worked flawlessly and the project was completed with zero non-conformances, making it an all-round success.
PRODUCTS USED IN THIS SOLUTION
Quick links
Ask an engineer