Legacy Way Tunnel, Brisbane
Creating efficiencies in smoke duct corbel anchorage through new technologies
The Challenge
![Thanks to the right anchors, the Legacy Way Tunnel was a success.](/content/hilti/A2/AU/en/engineering/design-center/anchor-systems/jobsite-references/legacy-way-tunnel--brisbane/_jcr_content/mainSection/mainColumn/image_text/image.img.1920.medium.jpeg)
Legacy Way in Brisbane is a 4.6 kilometre tunnel that connects the Western Freeway at Toowong with the Inner City Bypass (ICB) at Kelvin Grove.
The tunnel, constructed by Transcity JV, incorporates a smoke duct above the roadway for extraction in the event of a fire. This duct is formed from pre-cast panels, supported by a continuous corbel.
Construction of the smoke duct and corbel was the most extensive use of anchors in the tunnel's fit-out. The anchors consisted of 103,200 N20 reinforcing bars bonded 270 millimetres into the segment lining. Reinforcement was tied to these anchors before the corbel was cast.
![Herrenknecht rig and Hilti hammer drills and vacuums on the Legacy Way Tunnel in Brisbane](/content/hilti/A2/AU/en/engineering/design-center/anchor-systems/jobsite-references/legacy-way-tunnel--brisbane/_jcr_content/mainSection/mainColumn/two_image_text_col/left/image.img.1920.medium.jpeg)
Herrenknecht rig and Hilti hammer drills and vacuums on the Legacy Way Tunnel in Brisbane
![Smoke duct corbel on the Legacy Way Tunnel](/content/hilti/A2/AU/en/engineering/design-center/anchor-systems/jobsite-references/legacy-way-tunnel--brisbane/_jcr_content/mainSection/mainColumn/two_image_text_col/right/image.img.1920.medium.jpeg)
Smoke duct corbel on the Legacy Way Tunnel
Products used in this solution
Quick Links
Ask an engineer